Hi ,
I am getting error during my configuration
1,3,5 snapshot- You can see the error,It is showing Gigabit is not exist,& If you will see 5th image,Its showing In output/Generated/input folder “eth” file is not present,Why its happening.
for 2 snapshot-Why its telling Post build not supported,I did all configuration in gpt.
for 4 snapshot-In error ,Its telling we have not set wd0g0,and notification,But as you can see I did RE_Wdg_Cbk in notification,Why its so.
for 6,7 snapshot,You can see error for presalar,But I already set It,But one point,How we can enable predefined value(Showing in grey in 7th image).
How can i resolve these error,Please h
elp
Hi Nazni,
I see a lot of errors here, but overall i think it's because some nodes are lack of data/missing resources.
The reason of this is because it's not the correct version of RTD.
Please make sure to use the correct version RTD and also version of tools.
"I am working on S32K1XX_MCAL_4.3_RTM_1.0.5" >> I saw your project using RTM 1.0.4, so please try this release
Design : Product Download : Files (flexnetoperations.com)
Inside your project, .xdm files will be found and they contain information of the MCAL version that project uses, for me is S32K14X_MCAL4_3_RTM_1_0_1
And the plugin of the installed package should have the same information.
Are you possible to share your project or the .xdm configuration files for me?
So i can check it directly.
Thank you,
Nam.
Hi @Nazni
it would be nice to mention which device and which MCAL or RTD you have exactly. Also upload readable pictures. The uploaded ones are too small.
Regards,
Lukas