Enabling the macro in EB tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling the macro in EB tool

2,495 Views
Venu_M
Contributor III

Hello NXP team,

 

Can you please share the info how to enable the MACRO in EB tresos 29 version #define ADC_SAR_IP_EOC_ENABLED  for the ADC module S32K342 version.

0 Kudos
Reply
4 Replies

2,324 Views
Venu_M
Contributor III

Okay, Thanks Nam.

I already Enabled that EOC ISR.

Regards,
Venu

0 Kudos
Reply

2,394 Views
NamLee
NXP Employee
NXP Employee

Hi Venukumar,

I don't know exact version of the package that you using, but in S32K3 4.4 3.0.0 release version, there's no way to enable ADC_SAR_IP_EOC_ENABLED.

Could you please tell me the version of package and purpose of using this macro, so i can support you more?

Thank you,

Nam.

0 Kudos
Reply

2,376 Views
Venu_M
Contributor III

 

Hello Nam,

I'm using version  SW32K3_RTD_4.4_2.0.0

purpose of using this macro - EOC is used for EndOfConversion in ADC.

 

Thanks,

Venu

0 Kudos
Reply

2,343 Views
NamLee
NXP Employee
NXP Employee

Hi Venukumar,

Unfortunately, the macro ADC_SAR_IP_EOC_ENABLED can't be turned ON.

In case that you want to have a ISR when EOC of an ADC instance, let try this configuration for it.

NamLe_0-1686738614444.png

Thank you,

Nam.

0 Kudos
Reply