Emios interrupt on a Center Aligned Output PWM with Dead Time Insertion Buffered channel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Emios interrupt on a Center Aligned Output PWM with Dead Time Insertion Buffered channel

1,122 次查看
Alfredo_Rubio
Contributor II

I would like to implement an interrupt in a flank of an eMios channel that is operating under the Center Aligned Output PWM with Dead Time Insertion Buffered (OPWMCB) mode. It is possible to do it. I'm reading the Reference manual but haven't found the way to doit. I which register you confiture the interrupt functionality?

0 项奖励
回复
1 回复

1,103 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

eMIOS channel interrupt is enabled in channel Control register's FEN bit. If set (and DMA bit is cleared) interrupt request to core is triggered when Sn[FLAG] is set. 
In OPWMCB mode flag is set either on training edge or both edges, based on MODE field setting.

BR, Petr

0 项奖励
回复