EVB-S32K144 "error 7"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EVB-S32K144 "error 7"

2,471 Views
maufraistanguuy
Contributor II

Hello,

i'm actually working on the developement card S32k144 and since today i've got "error 7" in the file LASTSTAT.txt,

Because of that i can't use a program on the card

please help me 

Thanks.

There is the information about the card :

Board Name is: EVB-S32K144
MicroBoot Kernel Version is: 1.06
Bootloader Version is: 1.11
Installed Application: PEMicro EVB-S32K144 Mass Storage/Debug App
Application Version is: 1.19
DUID is: 65B33938-BFD581BF-374EE80B-BB68E678
EUID is: 6D31A239-2D77874D-184E0A18-A17168D6
TUID is: 74823938-47328196-8568CE18-22449847
TOA is: 86B6E505-1AFC9DA0-5C6655C3-7F4C3FA7
TOA2 is: 86B6E505-C076AEC6-01AE490C-C007E7CE
SUID is: 86B6E505-5F598197-37239804-8003EC65

Labels (1)
5 Replies

2,052 Views
hanraaijmakers
NXP Employee
NXP Employee

You can also get an error 7 when jumpers are not set correctly and the target is not powered because of that.

2,052 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

I have never seen error yet. Because the firmware in OpenSDA is from PEMicro, could you please contact PEMicro support directly?

P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools... 

Regards,

Martin

0 Kudos
Reply

2,052 Views
maufraistanguuy
Contributor II

Thanks for your answer

I've introduce my problem to PE micro but i'm still without answer

I would like to know if there is an other way than the USB port, to program the Evaluation bord ?

Maybe something with the SDA/JTAG port or the SWD port

Thanks

Regards,

Tanguuy

0 Kudos
Reply

2,052 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

yes, there are another ways. You can use some debug probe to load the code into the microcontroller. Please see the link below and check Emulators/Probes.

32-bit Automotive General Purpose MCUs|NXP 

All Universal Multilink and J-Link probes are compatibile with S32 Design Studio.

Could you please describe in detail what happen, when you connect your board via OpenSDA and click debug icon in S32 Design Studio? Did you receive any error?

Regards,

Martin

0 Kudos
Reply

2,052 Views
maufraistanguuy
Contributor II

Hello,

Thanks for your answer

i've just try to debug and before the software doesn't detect the card and now i've got a that say :" Device secure, erose to unsecure ?"

did you have any solution ?

Regards,

Tanguuy

0 Kudos
Reply