Hello,
i'm actually working on the developement card S32k144 and since today i've got "error 7" in the file LASTSTAT.txt,
Because of that i can't use a program on the card
please help me
Thanks.
There is the information about the card :
Board Name is: EVB-S32K144
MicroBoot Kernel Version is: 1.06
Bootloader Version is: 1.11
Installed Application: PEMicro EVB-S32K144 Mass Storage/Debug App
Application Version is: 1.19
DUID is: 65B33938-BFD581BF-374EE80B-BB68E678
EUID is: 6D31A239-2D77874D-184E0A18-A17168D6
TUID is: 74823938-47328196-8568CE18-22449847
TOA is: 86B6E505-1AFC9DA0-5C6655C3-7F4C3FA7
TOA2 is: 86B6E505-C076AEC6-01AE490C-C007E7CE
SUID is: 86B6E505-5F598197-37239804-8003EC65
You can also get an error 7 when jumpers are not set correctly and the target is not powered because of that.
Hello,
I have never seen error yet. Because the firmware in OpenSDA is from PEMicro, could you please contact PEMicro support directly?
Regards,
Martin
Thanks for your answer
I've introduce my problem to PE micro but i'm still without answer
I would like to know if there is an other way than the USB port, to program the Evaluation bord ?
Maybe something with the SDA/JTAG port or the SWD port
Thanks
Regards,
Tanguuy
Hello,
yes, there are another ways. You can use some debug probe to load the code into the microcontroller. Please see the link below and check Emulators/Probes.
32-bit Automotive General Purpose MCUs|NXP
All Universal Multilink and J-Link probes are compatibile with S32 Design Studio.
Could you please describe in detail what happen, when you connect your board via OpenSDA and click debug icon in S32 Design Studio? Did you receive any error?
Regards,
Martin
Hello,
Thanks for your answer
i've just try to debug and before the software doesn't detect the card and now i've got a that say :" Device secure, erose to unsecure ?"
did you have any solution ?
Regards,
Tanguuy