Thank you for your interest in our products and for contributing to our community.
Please refer to the following attached example:
It perform a PWM signal using the emios_0_ch_1_g (PTC1 - yellow signal) in OPWMB mode and using EMIOS_CH_23 in MCB mode as time base. Additionally, such PWM signal is routed through TRGMUX to lcu0_out0 (PTD3 - green signal) and lcu0_out1 (PTD2 - blue signal). Where lcu0_out0 replicates the PWM signal and lcu0_out1 inverts its output to feature complementary signals. Dead-time insertion is implemented with LUT rise/fall filters.

Please use S32DS 3.6, RTD 5.0.0 and S32K31XEVB-Q100.
If you need different SW and/or HW, you can create a new project, do manual config and code copy.
We hope this resolves your issue.
Best regards,
Leonardo