EBtresos activate code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EBtresos activate code

1,096 Views
jawen
Contributor I

您好,

 

我试图在 AUTOSAR 中使用 EBtresos,但未能激活。

 

激活代码 :B25C-AEBB-4319-BAB1

 

ERROR: flxActAppActivationSend (50040,41147,10248)
The quantity specified exceeds maximum quantity allowed (0).
Connection to FlexNet Operations Server failed.

 

因此,我需要另一个激活代码才能使用 EBtresos。

 

谢谢!

Tags (1)
0 Kudos
Reply
1 Reply

1,021 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Here is the reply from Flexnet Help:

Now, our team is in the process of updating the activation code information in the system. It will be reflected soon, but until then, please use the new activation code provided below:
F5CF-8A53-B979-CD50

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply