EB config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EB config

2,186 Views
PINKMAN
Contributor III

Hello, i 'm ready to learn how to config s32k MCAL by EB,  when i install SW32K1_RTD_4.4_1.0.0 ,i check the demo 

C:\NXP\SW32K1_RTD_4.4_1.0.0\eclipse\plugins\Can_TS_T40D2M10I0R0\examples\EBT\Can_example_S32K144

but after import the Can_example_S32K144 to EB,it report so many error that make me confused,can you help me to solve this issue as show in picture

thank you very much

9EEBFAA8-7356-4eed-A3B1-7DC74ADE6B9B.png

0 Kudos
Reply
3 Replies

2,130 Views
NamLee
NXP Employee
NXP Employee

Hi LXD,

I just checked around and in release note said that you need to use EB Tresos version 27.1.0

EB_Version.png

Thank you,

Nam.

0 Kudos
Reply

2,154 Views
NamLee
NXP Employee
NXP Employee

Hi LXD,

Did you install the correct version of EB? Could you please open Release note document of SW32K1_RTD_4.4_1.0.0 and check the required EB Version?

Thank you,

Nam.

0 Kudos
Reply

2,139 Views
PINKMAN
Contributor III
ok,i will check it ,thanks
0 Kudos
Reply