EB Tresos load configuration error with code TRESOSDB_10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EB Tresos load configuration error with code TRESOSDB_10

338 Views
lin2
Contributor I

Hi Community, 

When I load the existing projcet and double click to load configuration, the following error are encountered:

lin2_0-1751253510694.png

Could you please help me to understand what is going on? Other colleagues were able to load the project and the the configutation.

EB Tresos version is 26.2.0.

Thanks!

Best regards,

Lin

0 Kudos
Reply
2 Replies

324 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The error "corrupt system model" in EB Tresos typically indicates an issue with the project's configuration data, often due to inconsistencies or invalid data within the EB Tresos workspace.

The system model within EB Tresos stores information about the project's configuration, including modules, parameters, and relationships. If this data becomes corrupted or inconsistent (e.g., due to unexpected errors during saving, or manual modifications outside of the EB Tresos interface), the error can occur.

Try cleaning the project and rebuilding it. This can sometimes resolve inconsistencies in the build process.

But this is more question from EB support as the tresos is not NXP product. They will give you most accurate solution.

Best regards,

Peter

0 Kudos
Reply

312 Views
lin2
Contributor I

Hi Peter,

Thanks for you reply.

When I tried reinstall EB Tresos, and create a new workspace different from the deault one, the errors disappeared surprisingly. I guess this may result from the system situation and some other reasons that I don't know. Anyway, the problem has been solved. Thank you angin.

Best regards, 

Lin

0 Kudos
Reply