Does S32K3XX's FCCU compatible to FS4500's FCCU ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does S32K3XX's FCCU compatible to FS4500's FCCU ?

跳至解决方案
2,057 次查看
snaku_lee
Contributor III

Hi,

I have a question about the FCCU,

I know the recommend SBC for S32K3XX is FS26, but if I use FS45 as the PMIC to S32K, does their FCCU function are compatible?

Regards,

Snaku

0 项奖励
回复
1 解答
2,045 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Snaku,

The FCCU monitoring feature on FS26xyD devices is more complex.

For instance, it supports 8 different error protocols:

  • No monitoring
  • FCCU1 AND FCCU2 inputs monitoring activated by pair (Bi-stable protocol)
  • FCCU1 or FCCU2 single input level monitoring activated
  • FCCU1 input level monitoring only. FCCU2 input not used
  • FCCU2 input level monitoring only. FCCU1 input not used
  • FCCU1 or FCCU2 single input PWM monitoring activated
  • FCCU1 input PWM monitoring only, FCCU1 input level monitoring            
  • FCCU2 input PWM monitoring only, FCCU2 input level monitoring

Also various settings such as filtering time, error impact on Reset and Safety output is configurable by SPI.

For a detailed description, please take a closer look at chapter FCCU monitoring in the FS26 datasheet.

Please note that the FS26 is not a replacement of FS45/65, both devices are being sold and supported in parallel. They have different market targets and product position.

Capture.JPG

Best regards,

Tomas

 

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
949 次查看
Dflo
Contributor I

Hi Tomas,

I am using S32k311 and S32DS 3.5, can you tell me, if I want to use FCCU, which MCAL driver should I use?

0 项奖励
回复
2,046 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Snaku,

The FCCU monitoring feature on FS26xyD devices is more complex.

For instance, it supports 8 different error protocols:

  • No monitoring
  • FCCU1 AND FCCU2 inputs monitoring activated by pair (Bi-stable protocol)
  • FCCU1 or FCCU2 single input level monitoring activated
  • FCCU1 input level monitoring only. FCCU2 input not used
  • FCCU2 input level monitoring only. FCCU1 input not used
  • FCCU1 or FCCU2 single input PWM monitoring activated
  • FCCU1 input PWM monitoring only, FCCU1 input level monitoring            
  • FCCU2 input PWM monitoring only, FCCU2 input level monitoring

Also various settings such as filtering time, error impact on Reset and Safety output is configurable by SPI.

For a detailed description, please take a closer look at chapter FCCU monitoring in the FS26 datasheet.

Please note that the FS26 is not a replacement of FS45/65, both devices are being sold and supported in parallel. They have different market targets and product position.

Capture.JPG

Best regards,

Tomas

 

 

0 项奖励
回复
2,033 次查看
snaku_lee
Contributor III

Hi Tomas,

If our ECU safety requirement is ASIL-B, is there any concern for S32K324 + FS4500 ?

Regards,

Snaku

0 项奖励
回复
2,024 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Snaku,

The FCCU function is not a must for ASIL B system. So the FS45 ASIL B version does not support FCCU monitoring, ASIL D version of course yes. It can work together with the S32K324 MCU.

Best regards,

Tomas

0 项奖励
回复