Differential Signal acquisition

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Differential Signal acquisition

1,296 Views
abderrahmanaitg
Contributor I

Hi NXP Community,

I have to perform the acquisition of a differential signal (AP-AN) coming form an OPAMP using S32K 100pin MCU.

Both signals AN & AP are in the range of VREFH and VREFL. What is the best option to connect them to the MCU and reach the best accuracy:

Option 1: Use 2 adjacent pins, standard channels from different ADC module ADC0 and ADC1 

Option 2: Use 2 adjacent pins, precision channels from the same ADC module ADC0 or ADC1

Thank you in advance for your support.

Regards,

Abderrahman

0 Kudos
Reply
0 Replies