Default ISR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Default ISR

2,566 Views
Nayan123
Contributor II

Hii,

I am trying to run an simple led blinking program on FS32K144HAT0MLL Microcontroller which comes in S32 series.

But my application gets stuck in Default_ISR.

Previoulsy I was using FS32K144UAT0VLL, difference is the operating clock frequency and operating temperature range.

PFA of debug view.

Default_ISR.PNG

 

0 Kudos
Reply
2 Replies

2,556 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Nayan123,

Previous FS32K144UAT0VLL is 112MHz, and now FS32K144HAT0MLL is 80MHz. Did you change the clock frequency to 80MHz? 

According to debug window, seems that PINS_Init() caused hardfault Default_ISR. Before the codes access the PINS_Init related registers, did the clock gate enabled? for example: when you access PORT_PCRn check the CGC bit in PCC register.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,544 Views
Nayan123
Contributor II

Hii Robin_Shen,

Thank you for reaching out.

The issue is resolved by changing the crystal oscillator. Its position was incorrect.