Debugging while using external power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging while using external power

Jump to solution
2,153 Views
rjmalmeida0
Contributor III

Hi,

I'm using a S32K116 board. Can I debug using USB Open-SDA interface while powering from a 12V external source? I know that I need to change J107 to position 1-2, but I don't know if the USB will short with the externa power.

Thanks in advance.

Labels (1)
0 Kudos
Reply
1 Solution
2,065 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Rui Almeida, 

Yes, it is possible to debug with the on-board debugger while powering from a 12V external source. As you mentioned, you only need to change the position of J107 to 1-2 and connect the external power source and the USB cable.


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,066 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Rui Almeida, 

Yes, it is possible to debug with the on-board debugger while powering from a 12V external source. As you mentioned, you only need to change the position of J107 to 1-2 and connect the external power source and the USB cable.


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply