DMA SPI BARE METAL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DMA SPI BARE METAL

1,650件の閲覧回数
hajianik
Senior Contributor I

Hi,

Is there a bare metal example of BARE METAL DMA SPI on S32K14x series available anywhere?

Thanks,

Koorosh Hajiani

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,555件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Koorosh Hajiani, 

Unfortunately, we don't have any examples that meets these requirements. However, within the cookbook, you will find bare metal examples of SPI and DMA. You could use these examples as a starting point. 

Link to the application note: https://www.nxp.com/docs/en/application-note/AN5413.pdf 

Link to download the software: https://www.nxp.com/webapp/Download?colCode=AN5413SW&docLang=en 

Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信