D-Flash and P-Flash Memory Access and Programming in S32K118

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

D-Flash and P-Flash Memory Access and Programming in S32K118

4,351 Views
Arunpk
Contributor II

Hi,

I am currently using S32 Design Studio v3.4 with SDK version: s32sdk_s32k1xx_rtm_4.0.1.

I attempted to write data to D-Flash using the following API:

FLASH_DRV_Program(const flash_ssd_config_t *pSSDConfig, uint32_t dest, uint32_t size, const uint8_t *pData);
However, I am unable to write data to D-Flash. I’m not sure if there is a concept of unlocking/locking the memory regions before performing read/write operations.

I also tried using:

FLASH_DRV_SetDFlashProtection(const flash_ssd_config_t *pSSDConfig, uint8_t protectStatus);


But it returns STATUS_UNSUPPORTED.

I need help with the correct sequence of API calls and steps required to access and perform read/write operations on both D-Flash and P-Flash memory regions.

Additionally, if there is any UART-based Bootloader example code available for S32K118, please share it.

I'm also unsure whether any changes to the linker script are needed for this operation.

Please assist at the earliest.

Thank you!

0 Kudos
Reply
8 Replies

4,319 Views
Arunpk
Contributor II

Hi,

I am currently working on writing data to the D-Flash of the S32K118. However, during the FLASH_DRV_Init process, the D-Flash size is being detected as 0 Bytes, as shown in the code snippet below:

/* Temporary solution for FTFC and S32K144 CSEc part */
/* Get DEPART from Flash Configuration Register 1 */
DEPartitionCode = (uint8_t)((SIM->FCFG1 & SIM_FCFG1_DEPART_MASK) >> SIM_FCFG1_DEPART_SHIFT);

/* Get data flash size */
FLASH_DRV_GetDEPartitionCode(pSSDConfig, DEPartitionCode);

if (pSSDConfig->DFlashSize < FEATURE_FLS_DF_BLOCK_SIZE)
{
pSSDConfig->EEESize = FEATURE_FLS_FLEX_RAM_SIZE;
}
else
{
pSSDConfig->EEESize = 0U;
}
Due to this, I'm unable to perform read/write operations on the D-Flash. I also attempted to hardcode DEPartitionCode = 0, which results in the D-Flash size being set to 32KB, but when executing FLASH_DRV_CommandSequence(pSSDConfig), the MCU jumps to the DefaultISR.

I suspect the issue is related to the partitioning and configuration of the D-Flash memory region, possibly requiring a one-time setup or special procedure.

Could you please help me with the following:

  1. How can I enable or partition the full 32KB of D-Flash memory?
  2. Whether any additional configuration or one-time setup (e.g., using a specific tool or code sequence) is needed?
  3. If there are any constraints or dependencies based on DEPART/EEE settings?
  4. Do I need to update the linker file to support D-Flash access or memory mapping?

Your guidance or a reference example project for configuring and using D-Flash on S32K118 would be extremely helpful.

Thank you in advance for your support.

0 Kudos
Reply

4,305 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Arunpk 

If the FLASH_DRV_Init returns DFlash size 0, the device has been already partitioned and whole DFlash is used as a backup memory for Emulated EEPROM. To be able to use the DFlash directly, you need to remove the partition and then set new partition which will configure the DFlash as normal flash.

You can take a look at this example in SDK 4.0.1 folder:
c:\NXP\S32DS.3.5\S32DS\software\S32SDK_S32K1XX_RTM_4.0.1\examples\S32K118\driver_examples\system\flash_partitioning\

This example contains everything you need. To remove the partition (i.e. to erase whole device), you need to build the RAM target.
This will erase the device and partition, reprogram back the flash configuration field and then it will set the partition:

lukaszadrapa_0-1745508485341.png

 

To use whole DFlash as normal flash (so Emulated EEPROM is not used), use following parameters:

ret = FLASH_DRV_DEFlashPartition(&flashSSDConfig, 0x0Fu, 0x00u, 0x0u, false, true);

lukaszadrapa_3-1745508578776.png

lukaszadrapa_1-1745508500870.pnglukaszadrapa_2-1745508512763.png

 

The rest of the example then shows how to erase and program both PFlash and Dflash.

And one more thing - if CSEc was enabled in this device, FLASH_DRV_EraseAllBlock() function needed to remove the partition won't be successful. This command is blocked when CSEc is enabled. The only way to remove the partition is to run CMD_DBG_CHAL and CMD_DBG_AUTH commands with knowledge of MASTER_ECU_KEY. This is shown in following example:
c:\NXP\S32DS.3.5\S32DS\software\S32SDK_S32K1XX_RTM_4.0.1\examples\S32K118\driver_examples\system\csec_keyconfig\
Search for function eraseKeys().
If you don't know the MASTER_ECU_KEY, you are not allowed to remove the partition. There's no workaround for this.

lukaszadrapa_4-1745508651166.png

 

Regards,
Lukas

0 Kudos
Reply

3,927 Views
Arunpk
Contributor II

Hi Lukaszadrapa,

I am currently trying to run a bootloader (within 20KB in size) from D-Flash. From this bootloader, I am also attempting to write runtime data to the last sector of the same D-Flash, without performing any partitioning.

Writing to P-Flash works as expected. However, when writing to D-Flash, the first erase-and-write operation completes successfully. On the second attempt, during the erase operation, the system jumps to the DefaultISR handler.

Could you please help me resolve this issue? If this approach is incorrect, should I partition the D-Flash into two regions—one with 25KB for the bootloader and the other for storing runtime data?

If partitioning is required, could you also please provide the necessary steps or recommended procedure to do so?

Thank you in advance for your support.

Tags (1)
0 Kudos
Reply

3,892 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Arunpk 

If you want to program data flash, the code must run from either from RAM or from code flash. That's the only solution.

There's no feature which would split the data flash to two different RWW partitions.

Regards,

Lukas

0 Kudos
Reply

4,289 Views
Arunpk
Contributor II

Hi @lukaszadrapa ,

Thank you for your quick response.

I am now able to successfully write data to D-Flash using the FLASH_DRV_Program() API.

However, I am unsure which API should be used to read data from D-Flash and P-Flash. Could you please share the correct API or recommended method to read data from flash memory?

Thanks in advance for your support.

0 Kudos
Reply

4,280 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

There's no API for flash read. You can read the flash using pointers. Minimalist example:

unsigned int data;

data = *(unsigned int*)0x10000000; //read data from DFlash at 0x1000_0000

0 Kudos
Reply

4,199 Views
Arunpk
Contributor II

Hi @lukaszadrapa ,

I need assistance in partitioning the flash memory on the S32K118 as follows:

  • D-Flash → To store the bootloader and runtime data

  • P-Flash → To be divided into A/B partitions for firmware updates

Specifically, I’m looking for:

  1. I intend to receive the firmware image over UART and write it to either the A or B partition (passive partition) in P-Flash. However, I am unsure how to build the image in such a way that it can execute correctly from both A and B partitions(independent of its physical memory address). 
  2. An example linker script showing how to split both P-Flash and D-Flash into separate partitions.
  3. Any example projects or documentation references that could help with this setup.

Your guidance on these topics would be greatly appreciated.

Thank you,

0 Kudos
Reply

4,165 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

You can take a look at this application note:

https://www.nxp.com/docs/en/application-note/AN12323.pdf

https://www.nxp.com/docs/en/application-note-software/AN12323SW.zip

S32K11x has only one read partition in code flash, so follow example for S32K144. That means it is not possible to run "old "application in active block when updating passive block.

But notice that there's no HW support for AB swap and for remapping. Everything is up to user. The "partitioning" is done by user by adjusting of linker files.

Then be aware that S32 Design Studio does not support generation of PIE (position independent executable). As mentioned in the application note, IAR compiler supports it.

If you require HW support for AB swap and automatic remapping, take a look at S32K3 devices.

Regards,

Lukas

0 Kudos
Reply