Confusing about the MCAL QualityPackage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Confusing about the MCAL QualityPackage

2,065件の閲覧回数
VasilyWu
Contributor I

Hello,

I got the S32K1XX_MCAL_4.3_RTM_1.0.4_QualityPackage.zip from NXP.

Every module has individual quality files. 

When I am reading the AUTOSAR_MCAL_CAN_TraceabilityMatrix.xls, I have some confusion. 

Like this SWS_Can_00370, I know this requirement is from AutoSAR standards.

But like these CPR-MCAL-739.can, PR-MCAL-2696.can and SMCAL_SW035.can, where could I got those from?
What do CPR, PR, and SMCAL mean?
0 件の賞賛
返信
1 返信

2,047件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello,

These requirements are NXP sMCAL internal requirements, which are adapt with Safety MCAL concept and sMCAL coding convention. You can find description for these requirements in Description column. I don't think it's important to get in detail of CPR, PR and SMCAL meanings, since the description for each requirements is cleared.

Best Regards,

Nam

 

0 件の賞賛
返信