Cannot enter pin configuration for S32K338

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cannot enter pin configuration for S32K338

1,272件の閲覧回数
AW88
Contributor I

I am trying to simply enter the pin configuration tool for the S32K338 SOC. When creating a project, I can select the specific part number and package, but when I try to enter the Pin Configuration tool, I see an error that others have seen elsewhere stating MCU is Not Selected.

This is (to my knowledge) because the Project is blank. However, when I click the Project drop down and select my newly created project with the K338, a new error window pops open stating 'Opening the configuration failed due to an unknown reason.'

This error appears for any and all proejcts, even the Project_Pins_and_Clock_Training training project I've downloaded that has all files included.

I'm running S32DS 3.5.8 with what I think is everything needed to do this installed. I did however see that there is no SDK available to select when I first created the project...

0 件の賞賛
返信
0 返答(返信)