Can't install S32K3xx development package

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't install S32K3xx development package

920 次查看
HJLEE0403
Contributor I

I am currently using S32 Design Studio for S32 Platform version 3.5.0, and I am trying to update it using the offline package SW32_S32DS_3.5.14_D2409.zip.

However, when I attempt to install the S32K3xx Development Package (version 3.5.13), I encounter the following error:

I already have "GNU ARM PEMicro Interface Debugging Support" installed, but it seems this specific required feature ID is not recognized.스크린샷 2025-04-29 162134.png스크린샷 2025-04-29 164207.png

0 项奖励
回复
1 回复

894 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Which version of S32K3 RTD do you need to install?

It is recommended to uninstall S32DS and then reinstall it.

If you have problems installing S32K3 RTD 5.0.0, please refer to: HOWTO: offline install S32K3 RTD 4.0.0 in S32DS v3.5
1. Install S32Design Studio 3.5: S32DS.3.5_b220726_win32.x86_64.exe
2. Install Update 13 for S32DS: SW32_S32DS_3.5.13_D2407.zip
3. Install development package for S32K3XX: SW32K3_S32DS_3.5.13_D2407
4. Install development package for S32K396: SW32K39x_S32DS_3.5.13_D2407.zip
5. Install development package for S32M276: SW32M2_S32DS_3.5.13_D2407
6. Install updatesite for this release: SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.
zip


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复