Can S32K144 internal RTC wake up itself in VLPR or VLPS mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can S32K144 internal RTC wake up itself in VLPR or VLPS mode?

2,577 次查看
maoyuanluo
Contributor III

hi:

   Can S32K144 internal RTC wake up itself in VLPR or VLPS mode?

   What's the meaning of "The wakeup pin is not available for RTC on this device"?

   RTC.PNG

0 项奖励
回复
2 回复数

2,085 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The RTC module doesn’t wake up from VLPS, only from STOP1/2 modes. And it is functional in VLPR.

Please refer to Chapter 7.3.1 (Wake-up sources) and Table 35-4 (Module operation in available low power modes).

 

The wakeup pin is asserted when a RTC interrupt occurs.

But this pin is not available on S32K1xx.

 

Regards,

Daniel

0 项奖励
回复

2,085 次查看
jochengerster
NXP Employee
NXP Employee

HI Daniel,

to my understanding this will change with the documentation update end of Jan next year

best regards

Jochen

0 项奖励
回复