CSM and Crypto conflict

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CSM and Crypto conflict

2,275 次查看
Kanaqw
Contributor III

I have a problem when executing Csm_RandomGenerate and passing resultPtr parameter as local to a main function variable, as long as it goes to func Crypto_Cse_InitRng() it changes resultPtr to OutputPtr from configuration and writes random number there, but I dont get to return anything, only somehow access this variable from config later. Is it somekind of bug or am I doing something wrong?

0 项奖励
回复
3 回复数

2,256 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello @Kanaqw,

From our Crypto driver, Crypto_Cse_InitRng() function just initializes the seed, and Crypto_Cse_GenerateRnd() is the function which generates the random vector. In Crypto layer, these functions shall be called by Crypto_ProcessJob(), with the job service as CRYPTO_RANDOMGENERATE.

As a result, Csm_RandomGenerate() shall call Crypto_ProcessJob(), pass the job service as CRYPTO_RANDOMGENERATE, in order to call Crypto_Cse_GenerateRnd(). You can check the similar behavior in your stack, if Crypto_Cse_GenerateRnd(rndPtr) can be called and rndPtr has some values, then there must be some issues with Csm or the configuration, however we don't have any information of the Csm since we don't provide it. 

Best Regards,

Nam

0 项奖励
回复

2,268 次查看
Kanaqw
Contributor III

S32K146

0 项奖励
回复

2,269 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Kanaqw,

What device do you use?

 

 

0 项奖励
回复