CMP- Round Robin in NXP S32K144/142

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMP- Round Robin in NXP S32K144/142

2,738件の閲覧回数
mrugeshshah
Contributor I

Hello All
I am trying to use CMP in S32k142. I want to use two comparator channels in an alternate fashion (Continuous mode). I thought of using Round Robin method for two channels but then found out we can only trigger Round Robin for CMP in STOP mode. So is there any way or is it possible to trigger it RUN mode?

ラベル(1)
3 返答(返信)

2,583件の閲覧回数
razva_tilimpea
NXP Employee
NXP Employee

Hi,

As your understatement is right, round robin can be used only in STOP mode.

For your use case I see only one workaround: to implement the round robin in software with CMP module and an additional timer. Based on the overflow interrupt provided by timer you have to change the channel used for comparison and to check if the output value of the CMP matches expected value or not.

Best regards,

Razvan

2,583件の閲覧回数
mrugeshshah
Contributor I

Hi, 

Thanks for a quick response. I was doing the same switching the channels based on timer. I have one more question, as you said  output value of the CMP matches expected value or not, it means COUT bit? Is there any way to get input mux analog value which we are passing to comparator.   

0 件の賞賛
返信

2,583件の閲覧回数
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Yes, COUT is the result of the comparison. 

CMP don't convert the analog voltages to digital values. It works like an operational amplifier in open loop.

The only way to get the voltage value for some signals is to use ADC.

Best regards,

Razvan

0 件の賞賛
返信