Build Error when attempting to build example project "HvBms400_775_722_TPL_Bring_Up"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Build Error when attempting to build example project "HvBms400_775_722_TPL_Bring_Up"

2,544 次查看
wgthompson
Contributor II

Hello, I am attempting to build the example project HvBms400_775_722_TPL_Bring_Up but keep getting build errors around not being able to find include files or arm-none-eabi-gcc.exe errors. Also I am getting errors on my peripherals (specifically around Phy_665a) as attached to this post.

I have tried following the package addition order as described in this post with no luck. 

 

Please see attached for package installation details and errors found on my peripherals once I "update code"

Any help would be greatly appreciated. Thanks so much. 

  

20:21:22 **** Build of configuration Debug_FLASH for project HvBms400_775_722_TPL_Bring_Up_new ****
make -j12 all
Building file: ../src/Bjb.c
Building file: ../src/Cmu.c
Building file: ../src/Common.c
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@src/Bjb.args" -MMD -MP -MF"src/Bjb.d" -MT"src/Bjb.o" -o "src/Bjb.o" "../src/Bjb.c"
Invoking: Standard S32DS C Compiler
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@src/Bjb.args" -MMD -MP -MF"src/Cmu.d" -MT"src/Cmu.o" -o "src/Cmu.o" "../src/Cmu.c"
arm-none-eabi-gcc "@src/Bjb.args" -MMD -MP -MF"src/Common.d" -MT"src/Common.o" -o "src/Common.o" "../src/Common.c"
Building file: ../src/main.c
Building file: ../generate/src/Axbs_Ip_VS_0_PBcfg.c
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/generate/include: No such file or directory
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/RTD/include: No such file or directory
Building file: ../generate/src/CDD_Bcc_772c_Cfg.c
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/include: No such file or directory
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/generate/include: No such file or directory
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/RTD/include: No such file or directory
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/include: No such file or directory
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/generate/include: No such file or directory
arm-none-eabi-gcc "@src/Bjb.args" -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.c"
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/RTD/include: No such file or directory
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/include: No such file or directory
make: *** [src/subdir.mk:28: src/Bjb.o] Error 1
arm-none-eabi-gcc "@generate/src/Axbs_Ip_VS_0_PBcfg.args" -MMD -MP -MF"generate/src/CDD_Bcc_772c_Cfg.d" -MT"generate/src/CDD_Bcc_772c_Cfg.o" -o "generate/src/CDD_Bcc_772c_Cfg.o" "../generate/src/CDD_Bcc_772c_Cfg.c"
make: *** Waiting for unfinished jobs....
make: *** [src/subdir.mk:28: src/Cmu.o] Error 1
arm-none-eabi-gcc "@generate/src/Axbs_Ip_VS_0_PBcfg.args" -MMD -MP -MF"generate/src/Axbs_Ip_VS_0_PBcfg.d" -MT"generate/src/Axbs_Ip_VS_0_PBcfg.o" -o "generate/src/Axbs_Ip_VS_0_PBcfg.o" "../generate/src/Axbs_Ip_VS_0_PBcfg.c"
make: *** [src/subdir.mk:29: src/Common.o] Error 1
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/generate/include: No such file or directory
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/RTD/include: No such file or directory
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/include: No such file or directory
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/generate/include: No such file or directory
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/RTD/include: No such file or directory
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/include: No such file or directory
make: *** [src/subdir.mk:29: src/main.o] Error 1
make: *** [generate/src/subdir.mk:242: generate/src/CDD_Bcc_772c_Cfg.o] Error 1
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/generate/include: No such file or directory
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/RTD/include: No such file or directory
arm-none-eabi-gcc.exe: error: Thompson/workspaceS32DS.3.5/HvBms400_775_722_TPL_Bring_Up_new/include: No such file or directory
make: *** [generate/src/subdir.mk:242: generate/src/Axbs_Ip_VS_0_PBcfg.o] Error 1
"make -j12 all" terminated with exit code 2. Build might be incomplete.

20:21:22 Build Failed. 7 errors, 0 warnings. (took 637ms)

 

0 项奖励
回复
0 回复数