Bank switching for s32k microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bank switching for s32k microcontroller

3,987件の閲覧回数
snehitinaik_16
Contributor II

Hi,

I need few details for s32k microcontroller. Is the bank switch supported for s32k controller? I couldn't find this info in the controller manual. If Yes, can you please provide the sample code for the bank switch.

 

Thanks for support in advance.

 

タグ(3)
0 件の賞賛
返信
4 返答(返信)

3,960件の閲覧回数
snehitinaik_16
Contributor II

Thank You for the quick reply. Compiling the code with pic has some restriction with constants and constant pointers. Assuming we are able to successfully compile but how would the bank switch from A to B or vice versa occur during bootup work?

0 件の賞賛
返信

3,947件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

if you have S32K1, it's a matter of software, there's no hardware support for this. You can take a look at mentioned AN12323 to see how it is implemented.

Regards,

Lukas

0 件の賞賛
返信

3,946件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

... and I will add that bootloader is always started after reset and the bootloader decides which application will be executed.

0 件の賞賛
返信

3,976件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

S32K1xx does not support bank switching (memory mapping). If you want to do AB swap, it's necessary to either compile the projects as position independent or you need to track the versions and put them to correct place. We have this application note for S32K1 which implements AB swap:
https://www.nxp.com/docs/en/application-note/AN12323.pdf
https://www.nxp.com/docs/en/application-note-software/AN12323SW.zip
S32DS does not support PIE (position independent executable), it's necessary to use other compilers (like IAR as mentioned in the app note).

 

S32K3xx does have support for bank switching. Currently the A/B swap is supported by HSE firmware. You can take a look at the documentation of demo app:
c:\NXP\HSE_DEMOAPP_S32K3XX_0_1_2_0\HSE_DEMOAPP_S32K3XX_0_1_2_0_ReadMe.pdf
The HSE firmware and demo app can be installed from Standard Software:
https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-STDSW-D
And then there are some online trainings:
https://www.nxp.com/design/training/automotive-security-and-over-the-air-ota-solution-with-s32k3-mcu...
https://www.nxp.com/design/training/automotive-mcu-security-and-ota-solution-with-cost-optimized-s32...

Best Regards,

Ladislav