BLDC with s32k144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLDC with s32k144

2,655 Views
Abdel
Contributor II

Hi, can you help me to change rotation directory in Freemaster. I can only read a paramter rotationDir 0 (clockwise) or 1 (counterclockwise) but i can't control it. Or is there another parameter for it? Thank you in advance.

Best regards

Abdel

0 Kudos
Reply
3 Replies

2,645 Views
Abdel
Contributor II

Hi Petervlna,

thank you for your answer. I changed it in the code (macro) of course. But my question was, if i can change it in Freemaster, for example like the Switch between on and off. Thank you for your help.

Best regards

Abdel

0 Kudos
Reply

2,647 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

For BLDC there is only one rotation direction implemented in MCAT.

From freemaster of MCAT it is not possible to change direction.

If you like to change dirrection you have to change the macro (rotationDir) in to source code, compile it and load application to micro.

best regards,

Peter

 

0 Kudos
Reply

2,629 Views
Abdel
Contributor II

Hi Petervlna,

I hope you had a niceevening. The variable is determined to be read from a file, it is stored somewhere logically I can change the variable in a file from freemaster before I start the program. Is that correct?

Thank you in advance

Best regards

Abdel

0 Kudos
Reply