Auto MCU integrated TFT LCD Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Auto MCU integrated TFT LCD Driver

1,511 Views
Aidenchen
Contributor I

Product type is rotaryv shifter, it is with a TFT-LCD display screen

What we need:

As per below brief Hardware architecture:

  • MCU monitor rotary and buttons to actions to detect Driver desires, rotary detection shall be by Hall effect sensor, like TI TMAG5170-Q1.
  • MCU exchange info between Shifter and Vehicle over CAN bus.
  • MCU according to CAN message to control TFT-LCD display related images, so MCU must integrate with TFT-LCD driver module.
  • MCU Read Image data which stored in Flash over QSPI bus and control TFT-LCD screen image changing.

Please recommend us a Microcontroller which with:

  • CAN module
  • QSPI module
  • SPI module
  • TFT-LCD driver module
  • ADC, PWM, GPIO,
  • ISO 26262 functional safety level at least ASIL B.
  • Cyber security
  • Minimize footprint.
Tags (1)
0 Kudos
Reply
0 Replies