About UJA1169 that config NWP via CAN bus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About UJA1169 that config NWP via CAN bus

512件の閲覧回数
fedora
Contributor II

Hi,
The following sentence comes from the UJA1169A datasheet:

2.7 System control and diagnostic features
Watchdog period selectable between 8 ms and 4s supporting remote flash programming via the CAN bus

Please refer to the attached png file.

 

I don't understand how to support remote flash programming via the CAN bus?
Is it means that I can config the NWP(Nominal Watchdog Period of Watchdog control register) via other  devices on CAN bus?
Please help me explain it,thanks!

Best regards,

Fedora

 

タグ(2)
0 件の賞賛
返信
2 返答(返信)

482件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

No, it says that the UJA1169A allows to set a long watchdog period up to 4s so that the microcontroller can quite easily be flashed via the CAN bus, basically without having to consider the integrated watchdog.

BRs, Tomas

0 件の賞賛
返信

473件の閲覧回数
fedora
Contributor II

Oh, I understand it now.

Setting a long watchdog period that can quite easily upgrade the MCU firmware via the CAN bus.

Thank you, Tomas !

 

Best Regards,
Fedora

 

0 件の賞賛
返信