Hi [email protected],
The quick-write mode expects a number of bytes to be written.
1.
If the number of FlexRAM bytes allocated for EEPROM quick writes is:
FTFC->FCCOB[7] = 0x00;
FTFC->FCCOB[6] = 0x10; // 16 bytes
and there are only two 32-bit writes before reset, the brown-out code returned by the EEPROM quick write status query after the reset is:

And the two records are lost.
2.
Yes, that’s correct.
Once the expected number of bytes is reached, the EEPROM starts the maintenance on the flash block.
After that, subsequent data can be written as normal writes.
Please refer to AN11983, Appendix A EEPROM examples.
On p.22, there is a quick-write use case described.
“Quick write mode is intended to be used to save critical status records prior brownout events.”
Regards,
Daniel