AN12218SW java GUI Bootloader diagram

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN12218SW java GUI Bootloader diagram

Jump to solution
1,697 Views
mcristian
Contributor II

Hello,

I have the same problem ( Can't load IA 32-bit .dll on a AMD 64-bit platform) that was already some discussions regarding the GUI for UART bootloader:
Unable to run AN12218SW Bootloader (because of 32 bit dll) - NXP Community

I have a business laptop and IT department doesn't allow to install whatever I want and that's why I am not allow to install the old version of java

Because of this issue I want to create my custom GUI for bootloader. Is there any diagram or steps that I should when creating my interface? I saw in S32 Platform that the uC is answering sometimes with "0x41" or "0x45". How should my application interpret all those messages?

Thank you!

Tags (1)
0 Kudos
Reply
1 Solution
1,662 Views
nxp52415
NXP Employee
NXP Employee

Hello,

 

I think the information you are looking for can be found in the Application Note, more specifically in chapter 2.2.

AN12218: S32K1xx Bootloader – Application Note (nxp.com)

 

Regards

View solution in original post

0 Kudos
Reply
1 Reply
1,663 Views
nxp52415
NXP Employee
NXP Employee

Hello,

 

I think the information you are looking for can be found in the Application Note, more specifically in chapter 2.2.

AN12218: S32K1xx Bootloader – Application Note (nxp.com)

 

Regards

0 Kudos
Reply