ADKP Password Change

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADKP Password Change

974 Views
jeongwoo
Contributor I

Hello NXP,
We are using the S32K312 board.
We would like to know whether it is possible to change (or reset) the previously configured ADKP after Configuration Lock when the Life-Cycle is in the In-Field state.

Additionally, we would like to know whether it is possible to change the Life-Cycle from IN_FIELD to CUST_DEL.

0 Kudos
Reply
1 Reply

948 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Section 4.2.1 Configurable HSE system attributes of RM758227-RM00286 HSE-B Firmware Reference Manual - V2.7(2.7).pdf:
A set of programmable HSE system attributes within the secure NVM can be provisioned by the host via HSE administration services. Some of these attributes, once set, cannot be updated.
ADKP is listed in Table 16. One-time configurable HSE system attributes
Therefore, it is impossible to update ADKP anymore.
 
Page 17/299 states:
An LC transition is always one way. Reverting to a previous LC state is never possible.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 
0 Kudos
Reply