ADC syncronous conversion - Hardware Triggers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC syncronous conversion - Hardware Triggers

1,871件の閲覧回数
kyf
Contributor V

Hello NXP team !

Can someone explain me how this setup is like ??

 

kyf_0-1680522080503.pngkyf_0-1680522080503.png

Please also, can someone explain me how does the ADC0_EOC works ?

A. Is this trigger enabled in after every end of ADC0 channel conversion ?

B. When does the eDMA 0/1/16/17 trigger goes high in order to trigger the ADC12 NormalConv or SyncStartPulse ?

C. I want with 1 trigger to start a chain of conversion in ADC0 and ADC1. Which signal should I use to do this !? (the TRGMUX_IP_OUTPUT_ADC12_0_EXTRG_SYNC_START_PULSE or TRGMUX_IP_OUTPUT_ADC12_0_EXTRG_NORMAL_CONV ???

kyf_1-1680522150888.pngkyf_1-1680522150888.png

 

D. If I use a DMA channel to be triggered from BCTU or FIFO1. Can I use the same DMA to start a parallel Normal Conversion for ADC0 and ADC1 ?!

 

 

Kind regards,

kyf

0 件の賞賛
返信
1 返信

1,826件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your patient and your interest in our products and for using our community.

Regarding your questions…

A. Yes.
B. In both of them.
C. TRGMUX_IP_OUTPUT_ADC12_0_EXTRG_SYNC_START_PULSE

Hope it helps you.

Have a nice day!

0 件の賞賛
返信