ADC presampling with bypass sampling enabled - Not working - EBTressos

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC presampling with bypass sampling enabled - Not working - EBTressos

2,144件の閲覧回数
Venu_M
Contributor III

Hi,

I am trying to perform ADC conversion for precision input and standard input channels for S32K342 device with the following configurations.

  • Presample Enabled for each channel
  • Bypass sample enbled for whole HW unit
  • PREVAL - 0(VREFL)

Venukumar_0-1702621209869.pngVenukumar_0-1702621209869.png

 

OBSERVATION:

  • Observed PREVAL values in result register for the respective ADC channels.
  •  
    • if PREVAL - 1, Result registers are HIGH
      • Venukumar_2-1702621356140.pngVenukumar_2-1702621356140.png

         

    • if PREVAL - 0, Result register values are zeroes.
      • Venukumar_1-1702621281390.pngVenukumar_1-1702621281390.png

         

  •  
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,123件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Venu_M,

This is a correct observation.

When PSCR[PRECONV] = 0, pre-samling is followed by sampling and conversion.

When PSCR[PRECONV] = 1, pre-samling is followed by conversion.

RM, Section 61.3.9 Presampling

danielmartynek_0-1702652656148.pngdanielmartynek_0-1702652656148.png

 

BR, Daniel

 

0 件の賞賛
返信

2,080件の閲覧回数
Venu_M
Contributor III

Hi @danielmartynek ,

I am trying to get correct conversion data with PSCR[PRECONV] = 1. Not able to get the correct data.

Regards,
Venu

0 件の賞賛
返信

2,066件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Venu_M,

These are the correct data.

When PRECONV = 1, the sampling on the actual input channels is skipped.

 

BR, Daniel

 

0 件の賞賛
返信