ADC application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC application

2,235 Views
vinaykl
Contributor III

Hello,

I have a S32K144 EVK but I want to test Potentiometer using ADC application. But I dont know the process or procedures to read from API's provided in the components. I dont want to implement the example project given in SDK. Please help

0 Kudos
Reply
3 Replies

2,209 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

You can refer to the SDK examples (ADC Low Power, ADC Hardware Trigger, ADC PAL example and ADC Software Trigger) all of them use the potentiometer.

Hope it helps you.

Have a nice day!

0 Kudos
Reply

2,190 Views
vinaykl
Contributor III

Hi, Thanks for the response.

Will you please let me know in which SDK I will get these examples. Because I am using ARM 2.2 with SDK 3.0. I have used the given ADC example for S32K144 which is register level. I just want to implement using API's given in component inspector. Will you please help me solving this.?

 

0 Kudos
Reply

2,176 Views
_Leo_
NXP TechSupport
NXP TechSupport

The examples I mentioned to you are in the S32 Design Studio for S32 Platform (3.4), I recommend you using the latter IDE instead of the S32 Design Studio for Arm.

0 Kudos
Reply