ADC accuracy for the example code S32k118q048 evb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC accuracy for the example code S32k118q048 evb

723件の閲覧回数
yousefdessouki123
Contributor II

When working with one of the examples from the NXP cookbook, i reliased that the inaccuracy of the ADC channel conversion is very high. In the example code all conversions results for the voltages are shifted 1000 in terms of the final readings. For example when I connecte a 4V on the ADC pin, the voltage result after applying the scaling formula  is 5000. All readings suffer from this phenoma. Is there anything that could be done to mitigate such issue.

0 件の賞賛
返信
1 返信

710件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @yousefdessouki123,

You can refer to AN12217. Specifically, chapter 3 (Best practices to increase accuracy). 

Many factors can cause this, such as unstable VREF. You can also try to add an RC filter at the ADC input to suppress high-frequency noise. 

Best regards,
Julián.

0 件の賞賛
返信