ADC Code output Test on real time?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC Code output Test on real time?

1,100 Views
Turtledove
Contributor II

I am running example s32k148 on my s32 ide for arm. Please tell me how to check its output in real time expression and where to configure pins. I am new here in coding and on board.  Please guide me by mentioning steps.

ADC.c

/*
 * Copyright (c) 2014 - 2016, Freescale Semiconductor, Inc.
 * Copyright (c) 2016 - 2018, NXP.
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions are met:
 *
 * 1. Redistributions of source code must retain the above copyright notice,
 *    this list of conditions and the following disclaimer.
 *
 * 2. Redistributions in binary form must reproduce the above copyright notice,
 *    this list of conditions and the following disclaimer in the documentation
 *    and/or other materials provided with the distribution.
 *
 * 3. Neither the name of the copyright holder nor the names of its contributors
 *    may be used to endorse or promote products derived from this software
 *    without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY NXP "AS IS" AND ANY EXPRESSED OR
 * IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
 * OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
 * IN NO EVENT SHALL NXP OR ITS CONTRIBUTORS BE LIABLE FOR ANY DIRECT,
 * INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
 * (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
 * SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
 * HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT,
 * STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING
 * IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
 * THE POSSIBILITY OF SUCH DAMAGE.
 */
 
#include "ADC.h"
 
void ADC_init(void)
{
/*!
* ADC0 Clocking:
* ===================================================
*/
  PCC->PCCn[PCC_ADC0_INDEX] &=~ PCC_PCCn_CGC_MASK;  /* Disable clock to change PCS */
  PCC->PCCn[PCC_ADC0_INDEX] |= PCC_PCCn_PCS(1);     /* PCS=1: Select SOSCDIV2 */
  PCC->PCCn[PCC_ADC0_INDEX] |= PCC_PCCn_CGC_MASK;   /* Enable bus clock in ADC */
 
/*!
* ADC0 Initialization:
* ===================================================
*/
  ADC0->SC1[0] |= ADC_SC1_ADCH_MASK; /* ADCH=1F: Module is disabled for conversions */
                                    /* AIEN=0: Interrupts are disabled */
  ADC0->CFG1 |= ADC_CFG1_ADIV_MASK
     |ADC_CFG1_MODE(1); /* ADICLK=0: Input clk=ALTCLK1=SOSCDIV2 */
                                  /* ADIV=0: Prescaler=1 */
                                  /* MODE=1: 12-bit conversion */
 
  ADC0->CFG2 = ADC_CFG2_SMPLTS(12); /* SMPLTS=12(default): sample time is 13 ADC clks */
  ADC0->SC2 = 0x00000000;          /* ADTRG=0: SW trigger */
                                  /* ACFE,ACFGT,ACREN=0: Compare func disabled */
                                  /* DMAEN=0: DMA disabled */
                                    /* REFSEL=0: Voltage reference pins= VREFH, VREEFL */
  ADC0->SC3 = 0x00000000;        /* CAL=0: Do not start calibration sequence */
                                    /* ADCO=0: One conversion performed */
                                    /* AVGE,AVGS=0: HW average function disabled */
}
void ADC_init_HWTrigger(char Channel)  {
 
  PCC->PCCn[PCC_ADC0_INDEX] &=~ PCC_PCCn_CGC_MASK;  /* Disable clock to change PCS */
  PCC->PCCn[PCC_ADC0_INDEX] |= PCC_PCCn_PCS(1);     /* PCS=1: Select SOSCDIV2 */
  PCC->PCCn[PCC_ADC0_INDEX] |= PCC_PCCn_CGC_MASK;   /* Enable bus clock in ADC */
 
  ADC0->SC1[0] |= ADC_SC1_ADCH_MASK
              |ADC_SC1_AIEN_MASK;         /* ADCH=1F: Module is disabled for conversions*/
                                  /* AIEN=0: Interrupts are disabled */
  ADC0->CFG1 |= ADC_CFG1_ADIV_MASK
            |ADC_CFG1_MODE(1);/* ADICLK=0: Input clk=ALTCLK1=SOSCDIV2 */
                                  /* ADIV=0: Prescaler=1 */
                                  /* MODE=1: 12-bit conversion */
  ADC0->CFG2 = 0x00000000C;       /* SMPLTS=12(default): sample time is 13 ADC clks */
  ADC0->SC2 = ADC_SC2_ADTRG_MASK;         /* ADTRG=1: HW trigger */
                                  /* ACFE,ACFGT,ACREN=0: Compare func disabled */
                                  /* DMAEN=0: DMA disabled */
                                  /* REFSEL=0: Voltage reference pins= VREFH, VREEFL */
  ADC0->SC1[0] = ADC_SC1_ADCH(Channel)
      |ADC_SC1_AIEN_MASK;         /* ADCH=1F: Module is disabled for conversions*/
                                    /* AIEN=0: Interrupts are disabled */
  ADC0->SC3 = 0x00000000;         /* CAL=0: Do not start calibration sequence */
                                  /* ADCO=0: One conversion performed */
                                  /* AVGE,AVGS=0: HW average function disabled */
}
 
void convertAdcChan(uint16_t adcChan)
{
/*!
* For SW trigger mode, SC1[0] is used
* ===================================================
*/
  ADC0->SC1[0]&=~ADC_SC1_ADCH_MASK;       /* Clear prior ADCH bits */
  ADC0->SC1[0] = ADC_SC1_ADCH(adcChan);   /* Initiate Conversion */
}
 
uint8_t adc_complete(void)
{
  return ((ADC0->SC1[0] & ADC_SC1_COCO_MASK)>>ADC_SC1_COCO_SHIFT); /* Wait for completion */
}
 
uint32_t read_adc_chx(void)
{
  uint16_t adc_result=0;
  adc_result=ADC0->R[0];      /* For SW trigger mode, R[0] is used */
  return  (uint32_t) ((5000*adc_result)/0xFFF); /* Convert result to mv for 0-5V range */
}
 
 
ADC.h
 

#ifndef ADC_H_
#define ADC_H_
#include "device_registers.h" /* include peripheral declarations S32K144 */

void convertAdcChan(uint16_t);
void ADC_init(void);
void ADC_init_HWTrigger(char Channel);
uint8_t adc_complete(void);
uint32_t read_adc_chx(void);

#endif /* ADC_H_ */

0 Kudos
Reply
1 Reply

1,027 Views
_Leo_
NXP TechSupport
NXP TechSupport

Thank you for your interest in our products and for contributing to our community.

Please refer to the following knowledge base post:

S32M24x/S32K1 – FTM/TRGMUX/PDB/ADC – [RTD300] -> https://community.nxp.com/t5/S32M-Knowledge-Base/S32M24x-S32K1-FTM-TRGMUX-PDB-ADC-RTD300/ta-p/222903...

We hope this resolves your issue.

0 Kudos
Reply