ADC 2 instance for s32k344

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC 2 instance for s32k344

804件の閲覧回数
Ayaz
Contributor IV

Hi

I am triggering  the ADC at  each reload event of a pwm signal through the BCTU , the issue i am facing is that when i am triggering the ADC instance 2 at 40 kHz is working i can sample the data from the input , but when i am trying to sampling it at 2kHz there are no input , i do not have that issue at ADC 1 AND 2 instance, what do i miss here ?

i am using S32k344 .RTD 3.00

0 件の賞賛
返信
1 返信

780件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Ayaz

I can't give you a suitable solution from your description.

You need to provide a demo that can reproduce the problem so that we can help you

troubleshoot the cause of the problem.

0 件の賞賛
返信