32K144 clock configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

32K144 clock configuration

ソリューションへジャンプ
9,690件の閲覧回数
sarwath
Contributor IV

Hello Community,

1. what is the difference between core clock, system clock , bus clock and flash clock.

2. I configured the mcu with 48MHZ FIRC , 8 MHZ  SIRC and 40 MHZ SOSC (RUN MODE). System clock selector (FIRC_CLK). SPLL is disabled . check the below screenshot.

sarwath_0-1671620913729.png

3. Now in RUN mode (without SPLL), I can achieve upto 48 MHZ with FIRC. My question is If I want to achieve 80 MHZ what configuration I have to do.

4. SPLL CLK min is 90 MHZ and My MCU max clock is 80MHZ. So I disabled the SPLL.

Thanks in advance,

Sarwath

タグ(1)
0 件の賞賛
返信
1 解決策
9,640件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @sarwath 

The output frequency of the SPLL must be in range of 180 MHz - 320 MHz, the ones that can be configured in 80MHz are the SPLLDIV1_CLK and SPLLDIV2_CLK.

Refer to the image below which shows the settings I made:

VaneB_0-1672162154703.png

 

元の投稿で解決策を見る

9 返答(返信)
9,672件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @sarwath 

See section 27.3 Clock definitions of the S32K1xx MCU Family - Reference Manual. 
Regarding to the configuration of the clocks I suggest you use the Cloks tool from ConfigTools included in S32DS 3.4, where you can try different configurations to obtain the desired values.

 

B.R.

VaneB

0 件の賞賛
返信
9,667件の閲覧回数
sarwath
Contributor IV

Hello @VaneB ,

Thanks for your response.

I read the section 27.3 and I configured the clock in processor expert. 

sarwath_0-1671685883611.png

My S32K144 part number (FS32K144HFT0MLLR), its max clock speed is 80 MHZ. Currently I am configured to 48MHZ by FIRC_CLK. 

I tried to configure 80 MHZ with SPLL but I got warning due to SPLL min and max frequency. If I want achieve the 80 MHZ what configuration I have to do in processor expert clock settings.

sarwath_1-1671686272095.png

 

Thanks in advance,

Sarwath

0 件の賞賛
返信
9,652件の閲覧回数
sarwath
Contributor IV

Hello @VaneB ,

Any update for my clock setting query.

B.R,

Sarwath

0 件の賞賛
返信
9,641件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @sarwath 

The output frequency of the SPLL must be in range of 180 MHz - 320 MHz, the ones that can be configured in 80MHz are the SPLLDIV1_CLK and SPLLDIV2_CLK.

Refer to the image below which shows the settings I made:

VaneB_0-1672162154703.png

 

9,631件の閲覧回数
sarwath
Contributor IV

Thanks @VaneB  . I'm just curious which IDE you're using. I'm using the S32DS IDE, and I don't see any clock setting GUIs like yours.

0 件の賞賛
返信
9,622件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @sarwath 

It is the clock tool included in Config Tools.

VaneB_0-1672241197528.png

 

0 件の賞賛
返信
9,610件の閲覧回数
sarwath
Contributor IV

Hi @VaneB,

Why are my S32DS options so different from yours? I have the processor expert instead of config tools.

sarwath_0-1672309711608.png

 

 

0 件の賞賛
返信
9,598件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @sarwath 

It is because the version is S32 Design Studio 3.4 – Windows/Linux 

0 件の賞賛
返信
9,608件の閲覧回数
sarwath
Contributor IV

Hi @VaneB ,

S32k144 part number : FS32K144HAT0MLLT

 I understood how to run my MCU @80Mhz. Now I want to change the system clock source because the FIRC is selected as the system clock source by default (48MHz).

how to modify the system clock source to select the SPLL as source.

I thought the below instruction will set SPLL as system clock source

//Configure the system clock source and dividers, depending on power mode
SCG->RCCR =

SCG_RCCR_SCS(6)|SCG_RCCR_DIVCORE(1)|SCG_RCCR_DIVBUS(1)|SCG_RCCR_DIVSLOW(2);

But I am not getting SPLL as system clock source.

sarwath_0-1672315228521.png

 

In all examples they following instructions are used to set clocks,

sarwath_1-1672315285844.png

If I use above code to set the clocks I am getting hard fault.  I want to know why the above clock settings is not working for me.

Thanks in advance,

Sarwath

 

0 件の賞賛
返信