Example S32K324 STANDBY wake up using GPIO Switch DS3.5 RTD300

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example S32K324 STANDBY wake up using GPIO Switch DS3.5 RTD300

Example S32K324 STANDBY wake up using GPIO Switch DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of the
 POWER & WKUP IP Driver for the S32K3xx MCU.

In current example :--
SW-5 = PTB-26  -----> PRESS to enter the STANDBY mode.
SW-6 = PTB-19 = WKUP[38] --> PRESS to exit the STANDBY mode.

The example uses PIT-0 timer, to generate the periodic interrupt.

 ------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-T172
* MCU: S32K324
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

Push Buttons :---

Dinesh_Guleria_4-1719231631866.png

 

 

Dinesh_Guleria_3-1719231563667.png


Wake-up source, SW-6 GPIO:--

Dinesh_Guleria_5-1719231808719.png

 

 



********* If you use external BJT on your board to generate 1.5 volts *******************

Dinesh_Guleria_1-1719231351206.png
 

I tested on Our T172 EVB, with NPN external Ballast transistor is selected to supply the V15_MCU domain. I am able to wake up from standby mode.

If we select 2-3 in J31 then NPN external Ballast transistor is selected to supply the V15_MCU domain & wakeup is ok on T172 EVB

You have to make following settings in code :--

Dinesh_Guleria_2-1719231402148.png

 

Dinesh_Guleria_0-1719231338249.png

 

 

附件
无评分
版本历史
最后更新:
‎06-24-2024 05:27 AM
更新人: