Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300

Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of the FEE MCAL Driver for the S32K3xx MCU.

This example read & write 4 byte FEE BLock.
I have renamed the FEE block using a MACRO as FOUR_BYTE_EEPROM_FEE_VARIABLE.

The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x52_0000 .


 ------------------------------------------------------------------------------
* Test HW: S32K3X2EVB-Q172
* MCU: S32K312
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

Dinesh_Guleria_0-1716470300913.png

 

 

Attachments
Comments

Pe Micro use to delete the Dataflash, on every new FLashing of firmware, which corrupts the EEPROM data.

After making this changes in debug configuration it worked..

Dinesh_Guleria_0-1719396133457.png

 

Dinesh_Guleria_1-1719396155702.png

 

 

Dinesh_Guleria_2-1719396179846.png

 

 

No ratings
Version history
Last update:
‎06-12-2024 11:16 PM
Updated by: