update s32g kernel

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

update s32g kernel

2,098 次查看
lily95
Contributor I

Hello everyone:

Now i have a question, i want to update the kernel version from 4.19 to 5.1 on the board NXP S32G274A-RDB. The info of the board are :

CPU: NXP S32G274A rev. 2.1.0
Reset cause: Power-On Reset
Model: NXP S32G27x
Board: NXP S32G274A-RDB

 

i want to know where can i get the support about the kernel updating of S32G274A-RDB, like doc and SDK etc. 

THANKS for any suggestions.

0 项奖励
回复
1 回复

2,085 次查看
bpe
NXP Employee
NXP Employee

If you want to stay with an NXP-verified kernel, consider moving to the most
recent Automotive BSP which supports two kernel versions, 5.4 and 5.10.
Use Automotive Software Package Manager to obtain the installation package.
See Automotive BSP User Manual which is part of the same installation package
for installation and usage instructions.

As of Linux kernel version 5.1, there are no BSPs for your development board
built around it. If you are to move to that kernel by yourself, what you
can start with is generic Yocto documentation discussing kernel-related
tasks:

https://docs.yoctoproject.org/dev-manual/common-tasks.html#adding-a-kernel-for-the-machine

https://docs.yoctoproject.org/kernel-dev/index.html

Note that we can provide a very limited support to non-SDK kernels.

Best Regards,
Platon

 

0 项奖励
回复