s32g3 multicore enable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32g3 multicore enable

5,052 次查看
pupu_ji
Contributor II

Hi, all

I refer "Enabling Multicore Application on S32G2using S32G2 Platform Software Integration" to use it on s32g3.

Building U-Boot use "s32g399ardb3_defconfig" ,and generate fin.32 as described in the "Linux BSP 35.0 User Manual for S32G3 platforms"  ,changing 'FIP_ALIGN := 16'  to 'FIP_ALIGN := 64', adding FIP_QSPI_OFFSET=<QSPI offset> make parameter . The log  as follow:

pupu_ji_0-1687852851085.png

pupu_ji_1-1687852866238.png

But when use the dd if=fip.s32 of=/dev/sdb skip=512 seek=512 iflag=skip_bytes oflag=seek_bytes
conv=fsync,notrunc copy fip.32 to SD card , the SD card will become garbled. Can't copy else file.

If I copy them  directly to SD card , nothing on the terminal.

Could you help me?

 

0 项奖励
回复
7 回复数

5,038 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We have made the modifications to have the FIP_ALIGN:=64 and replaced the fip.s32 file by using the following command:

DanielAguirre_0-1687890541422.png

We are not seeing any problem on regards of this configuration. One difference is that we are not adding any "FIP_QSPI_OFFSET" to the make command.

DanielAguirre_2-1687890692495.png

You cannot just copy the fip.s32 directly to your SD card, you need to replace the fip section inside the image for it to work.

Before replacing the fip.s32 file, was your image working?

Please, let us know.

0 项奖励
回复

5,023 次查看
pupu_ji
Contributor II

Thanks for your reply. ><

pupu_ji_0-1687945614337.png

 

My SD card has two partition: "boot_s32g39" and "fsl-image-auto-s".

I copy fip.32 to fsl-image-auto-s using the command, and it seems good.

SW4-7 ON, (boot from sd card) is working.

pupu_ji_1-1687918175152.png

But nothing is on the uart when SW4 is all OFF(boot from nor flash).

Did I do something wrong?  Help me,plead.  TOT.

Copied ipc.ko to SD card boot_s32g39.

pupu_ji_8-1687918577423.png

Used s32ds flash tool to load bt_m7_blob.bin , fip.bin and IPCF.bin. 

pupu_ji_2-1687918297935.png

pupu_ji_3-1687918308355.pngpupu_ji_4-1687918320062.png

 

 

0 项奖励
回复

4,991 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For what you have shown, it seems that the fip.s32 file was made correctly. In order to verify the fip.bin, you can create an IVT where A53_0 is the boot core, fip.bin is the application bootloader and select QSPI as boot interface (adding the configuration parameters to increase the speed of the interface).

If the fip.bin was created correctly, then you should be able to boot from QSPI and see a Linux terminal as the one you are seeing under your SD boot mode. Just as a note, fip.s32 also needs to be replaced on your SD (as you have already done). You cannot use fip.bin with an image that does not have the fip.s32 file modified.

The example mentioned above is still not a multicore application but will let us confirm if the fip.bin was also generated correctly.

Please, let us know.

0 项奖励
回复

4,960 次查看
pupu_ji
Contributor II

Hi, I tried the method you mentioned, created an INV where A53_0 is the boot core, but it failed. Does it indicate that the fip.bin was created incorrectly? But fin.bin and fin.32 was created at same time at /arm-trusted-firmware/build/s32g399/release. There is a question , how to prove that fip.32 was indeed copied successfully? I can' find fip.32 in my SD card "fsl-image-auto-s" partition.

pupu_ji_0-1688016302538.png

 

0 项奖励
回复

4,949 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. We remember that you added the FIP_QSPI_OFFSET variable to your make command, we did not.

Have you tried running the make command without it? We can see an output on the terminal with the IVT + A53_0 boot + QSPI + (App_BL -> fip.bin).

Also, which RAM start pointer and entry pointer did you use? We remembered you share the ATF output log, but which addresses did you use and where?

As to proof if fip.s32 has been copied, you will not see it directly in the SD partition. You might need to do a HEX dump and compare to see if the fip.s32 section was indeed modified.

Please, let us know.

0 项奖励
回复

4,881 次查看
pupu_ji
Contributor II

Hi,

I tried command without FIP_QSPI_OFFSET, still failed.

pupu_ji_0-1688525708555.png

"Also, which RAM start pointer and entry pointer did you use? We remembered you share the ATF output log, but which addresses did you use and where?"

I used

entry point ->reset handler address

load address ->load image at address(RAM)

pupu_ji_0-1688537327303.pngpupu_ji_1-1688537333282.png

 

 

 

 

 

And could you provide the files for me to try it ?

 

 

 

 

 

0 项奖励
回复

4,859 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

One you created fip.bin without the QSPI offset, which addresses are you using for the IVT structure (RAM start address; RAM entry address)?

DanielAguirre_0-1688580406536.png

We are still referring to the non-multicore boot, which selects A53_0 core as the boot core and the fip.bin as the Application Bootloader.

Also, did you add QSPI parameters to increase the speed of the interface?

We see that you are still using the bootloader for the fip.bin, have you tried to boot the A53_0 without the bootloader?

As for sharing files, help us opening a ticket under the NXP online services, since we do not commonly share files through the community.

Please, let us know.

0 项奖励
回复