s32 M7 bootloader to load u-boot for A53

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32 M7 bootloader to load u-boot for A53

3,902 次查看
vip_mistry
Contributor I

I want to build M7 bootloader that can load u-boot on a53_0 for s32g. Can you guide me with design steps to build M7 bootloader for the same. 

I have built u-boot.bin and u-boot.s32 for BSP 27. 

0 项奖励
回复
2 回复数

3,874 次查看
bpe
NXP Employee
NXP Employee

The software you are requesting for is part of NXP Platform Software
Integration for S32G2XX package. Follow this link to enter the download
procedure and select Automotive SW – S32G2 Reference Software then
Automotive SW - S32G2 - Integration Reference Examples to obtain it.

Further details can be found in Bootloader Integration Example User Manual
which is part of the package mentioned above.

There is also a nice multicore boot demo based on the same Integration
bootloader, however, it is currently available only after an approval. If you wish
to obtain it: (a) register yourself on NXP Website with your corporate
account; (b) open a Support Case.

Best Regards,
Platon

 

0 项奖励
回复

3,306 次查看
nadeem
Contributor I

Dear Sir,

I was able to find the :-

 Automotive SW – S32G2 Reference Software then
Automotive SW - S32G2 - Integration Reference Examples

However when I try to import the reference design for Lighting, I noticed the only project available is Tresos, and there is no /applications/realtime/S32DS/workspaces/Lighting_<platform>_<version>.

I only can find the :-C:\NXP\Platform_Software_Integration_S32G2XX_2021_07\applications\realtime\tresos\ 

However this seems to be incorrect as it needs Tresos, I also checked :-C:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32XX_2022_03.  

the /PlatformSoftwareIntegration/ folder does not exist.

Please can you advise what I may be doing wrong.

thanking you,

Nadeem Jamal

 

 

 

0 项奖励
回复