pfe2 sgmii setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pfe2 sgmii setup

918件の閲覧回数
shiyiheng
Contributor III

The RDB3 development board I use is developed based on BSP34 branch, and I want to configure pfe2 as sgmii. After looking at the schematic diagram, I find that the configuration can be done in the following ways, but how can I distinguish 1.25g from 3.125g? How can I configure hwconfig in these two cases?

shiyiheng_0-1727146780133.png

 

0 件の賞賛
返信
1 返信

880件の閲覧回数
chenyin_h
NXP Employee
NXP Employee

Hello, @shiyiheng 

Thanks for your post.

For serdes0(mode3), it is not mentioned in the BSP 34 UM, but the following combination is supported on RDB3 based on latest BSP.

chenyin_h_0-1727244979815.png

You may refernece it for details.

 

 

BR

Chenyin

0 件の賞賛
返信