difference between BCAN and FlexCAN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

difference between BCAN and FlexCAN

跳至解决方案
2,854 次查看
skseofh
Contributor II

Hi

I'm using S32G2 chipset.

 

What is difference between BCAN and FlexCAN?

0 项奖励
回复
1 解答
2,839 次查看
bpe
NXP Employee
NXP Employee


The main difference between FlexCAN and BCAN is that the latter is controlled
by LLCE, a microcode-driven multiple core engine. The main advantage of
FlexCAN which is a pure HW, is simplicity and the option to use it as the boot
device. LLCE-controlled BCAN offers a simpler, fire-and-forget programming
model, more flexible buffer management, advanced GPP core offload services:
security (authentication and enc/dec), interworking with PFE Ethernet,
automatic CAN message forwarding. See S32G3 Reference Manual, Chapter 54 for
more information on LLCE.

Best Regards,
Platon

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,840 次查看
bpe
NXP Employee
NXP Employee


The main difference between FlexCAN and BCAN is that the latter is controlled
by LLCE, a microcode-driven multiple core engine. The main advantage of
FlexCAN which is a pure HW, is simplicity and the option to use it as the boot
device. LLCE-controlled BCAN offers a simpler, fire-and-forget programming
model, more flexible buffer management, advanced GPP core offload services:
security (authentication and enc/dec), interworking with PFE Ethernet,
automatic CAN message forwarding. See S32G3 Reference Manual, Chapter 54 for
more information on LLCE.

Best Regards,
Platon

 

0 项奖励
回复