difference between BCAN and FlexCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

difference between BCAN and FlexCAN

ソリューションへジャンプ
2,854件の閲覧回数
skseofh
Contributor II

Hi

I'm using S32G2 chipset.

 

What is difference between BCAN and FlexCAN?

0 件の賞賛
返信
1 解決策
2,839件の閲覧回数
bpe
NXP Employee
NXP Employee


The main difference between FlexCAN and BCAN is that the latter is controlled
by LLCE, a microcode-driven multiple core engine. The main advantage of
FlexCAN which is a pure HW, is simplicity and the option to use it as the boot
device. LLCE-controlled BCAN offers a simpler, fire-and-forget programming
model, more flexible buffer management, advanced GPP core offload services:
security (authentication and enc/dec), interworking with PFE Ethernet,
automatic CAN message forwarding. See S32G3 Reference Manual, Chapter 54 for
more information on LLCE.

Best Regards,
Platon

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,840件の閲覧回数
bpe
NXP Employee
NXP Employee


The main difference between FlexCAN and BCAN is that the latter is controlled
by LLCE, a microcode-driven multiple core engine. The main advantage of
FlexCAN which is a pure HW, is simplicity and the option to use it as the boot
device. LLCE-controlled BCAN offers a simpler, fire-and-forget programming
model, more flexible buffer management, advanced GPP core offload services:
security (authentication and enc/dec), interworking with PFE Ethernet,
automatic CAN message forwarding. See S32G3 Reference Manual, Chapter 54 for
more information on LLCE.

Best Regards,
Platon

 

0 件の賞賛
返信