about the efuse read limitation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about the efuse read limitation

ソリューションへジャンプ
859件の閲覧回数
brian_w
Contributor III

Hi,

 In the G2 rm, it's said the read limitation is 20m times per bit.

brian_w_0-1684756923339.png

 After every standby mode exist, there will be a destructive reset and the efuse need to be read again. If G2 swtiches between standby mode and fast boot mode frequently, after some time, the efuse will have problem?

 How should I avoid to damage the efuse?

0 件の賞賛
返信
1 解決策
846件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

If the accumulative reads to a specific bit surpasses 2 million reads, we cannot longer confirm the correct functioning on regards of the read operation under the eFuses (which should be around 550 reads per day under a 10-year lifespan, under a single bit).

Since this is part of platform, there is no plan or document on how to avoid damage to the eFuse. One possibility is to have a copy of the fuses on an external EEPROM, for redundancy.

Please, let us know.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
847件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

If the accumulative reads to a specific bit surpasses 2 million reads, we cannot longer confirm the correct functioning on regards of the read operation under the eFuses (which should be around 550 reads per day under a 10-year lifespan, under a single bit).

Since this is part of platform, there is no plan or document on how to avoid damage to the eFuse. One possibility is to have a copy of the fuses on an external EEPROM, for redundancy.

Please, let us know.

0 件の賞賛
返信