about the efuse read limitation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

about the efuse read limitation

跳至解决方案
758 次查看
brian_w
Contributor III

Hi,

 In the G2 rm, it's said the read limitation is 20m times per bit.

brian_w_0-1684756923339.png

 After every standby mode exist, there will be a destructive reset and the efuse need to be read again. If G2 swtiches between standby mode and fast boot mode frequently, after some time, the efuse will have problem?

 How should I avoid to damage the efuse?

0 项奖励
回复
1 解答
745 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

If the accumulative reads to a specific bit surpasses 2 million reads, we cannot longer confirm the correct functioning on regards of the read operation under the eFuses (which should be around 550 reads per day under a 10-year lifespan, under a single bit).

Since this is part of platform, there is no plan or document on how to avoid damage to the eFuse. One possibility is to have a copy of the fuses on an external EEPROM, for redundancy.

Please, let us know.

在原帖中查看解决方案

0 项奖励
回复
1 回复
746 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

If the accumulative reads to a specific bit surpasses 2 million reads, we cannot longer confirm the correct functioning on regards of the read operation under the eFuses (which should be around 550 reads per day under a 10-year lifespan, under a single bit).

Since this is part of platform, there is no plan or document on how to avoid damage to the eFuse. One possibility is to have a copy of the fuses on an external EEPROM, for redundancy.

Please, let us know.

0 项奖励
回复