a53_sys_scst_loadstore_test7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

a53_sys_scst_loadstore_test7

Jump to solution
2,330 Views
nmansour
Contributor I

Hello, 

we're using SCST_A53_S32G_RFP_2.0.2 library for A53 runtime tests. 

Currently we have an issue in running test: a53_sys_scst_loadstore_test7 and it returns Error Code: ERR_SCST_FAILED_A53_C3

in the user manual it's mentioned to have specific access rights by the MMU: 

2026-04-08 14_26_05-A53_S32G_SCST_User_Manual.pdf - Adobe Acrobat Reader (64-bit).png

Could you provide an example on how this mapping is expected by the test or in MMU configuration since the MMU only accepts "address ranges" not section names? Also Could you clarify why the test is failing currently?

Thanks in advance for your support.

Tags (1)
0 Kudos
Reply
1 Solution
1,042 Views

Input from Yi Yang:

This is known issue. Test ID=59 can not be executed under QNX. Only range of tests 0-58 can be executed. Please see Application Note for more details. AN13294

 

We can close the ticket.

View solution in original post

0 Kudos
Reply
6 Replies
2,068 Views
nmansour
Contributor I

Hi @al thanks for the reply 

I've checked the provided Demo and i have a couple of questions hope you can clarify. 

- On the demo, it depends on the linker section allocation in the linker file. 
This option we cannot use because the runtime tests are compiled and linked in the PH application and linking is done by the QNX. 
So is there a workaround for this?

- in the file you mentioned to check A53_SYS_SCST_RAM_DATA_TARGET0_VADDR this one we currently don't have defined any my understanding is that we either use the virtual address macro or the linker section. Could this be a substitute? 
- in the user manual what does it mean exactly by proper MMU mapping, is it only the attributes or something else is missing? for EL1 mmu configuration, this is handled by QNX so we can't change it. 
 

0 Kudos
Reply
1,423 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @nmansour,

Please find my answers in the private message I sent you.

 

Regards

0 Kudos
Reply
1,043 Views

Input from Yi Yang:

This is known issue. Test ID=59 can not be executed under QNX. Only range of tests 0-58 can be executed. Please see Application Note for more details. AN13294

 

We can close the ticket.

0 Kudos
Reply
2,058 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @nmansour,

Doing some more investigation on the SCST topic I was able to find this document QNX Integration Example of S32G A53 SCST Library. That should help you exactly with what you are looking for.

Specifically about your questions, support for QNX is outside the scope of the support we offer in this community, so I would recommend reaching out to the QNX vendor for support.

 

Let me know if I can help you with anything else.

0 Kudos
Reply
2,050 Views
nmansour
Contributor I
Thanks for the quick reply.
Could you also give some insights on using the VADDR instead of the linker section?
Where can i find this explained?
A53_SYS_SCST_RAM_DATA_TARGET0_VADDR

for these 2 points in particular:
- in the file you mentioned to check A53_SYS_SCST_RAM_DATA_TARGET0_VADDR this one we currently don't have defined any my understanding is that we either use the virtual address macro or the linker section. Could this be a substitute?
- in the user manual what does it mean exactly by proper MMU mapping, is it only the attributes or something else is missing?


0 Kudos
Reply
2,305 Views
alejandro_e
NXP TechSupport
NXP TechSupport

Hello @nmansour,

Thanks for reaching out to us. About your questions, we do have an example on how to configure MMU selections, it is called A53 SCST Linux Integration Demo, once you install it you can check function mmu_init() in C:\NXP\SCST_FW_A53_S32G_1.0\scst_fw\src\mmu_config.c, in that function you can see how to initialize memory ranges. As you will see it uses the names of the sections instead of the explicit values, however those names get resolved into values at compile time.

Regarding the possible reasons for the failing result, please check what is mentioned for the A53_SYS_SCST_RAM_DATA_TARGET0_VADDR definition, in C:\NXP\SCST_A53_S32G_RFP_2.0.2\SCST_SYS\src\h\a53_sys_scst_configuration.h.

 

You can downloading the demo I mentioned by following these steps:

- go to https://www.nxp.com/ and log into your account

- Go to "My NXP Account" and then on "Software Licensing and Support":

Screenshot 2026-04-08 143902.png

Screenshot 2026-04-08 143956.png

 

- Now click on "View accounts", this will take you to the FlexNet portal, where you should be able to see all your available products.

Screenshot 2026-04-08 144259.png

Screenshot 2026-04-08 145044.png

- Now got to: Automotive SW – S32G Reference Software and then Automotive SW - S32G A53 SCST Linux Integration Demo. Download de executable file and Screenshot 2026-04-08 145425.png

After executing said file you will be able to find the example I mentioned above.

 

 Let me know if you have more questions.

0 Kudos
Reply