Hi,sdx111
Thank you for your reply.
PB_07 is used for the KSZ_A_INF_B to connect the PHY, INT/PME_2 is the "Interrupt Output / Wake-up Output (PME)" pin of KSZ9031, the signal is transmitted from PHY to SOC.
The definition of this pin was not found in the device tree. This might be because the MDIO polling function of the PHY was implemented, the interrupt function of the PHY was not implemented.
Joey_z_2-1770708982073.png
Joey_z_1-1770708739993.png
What state do you want PB_07 to maintain? PB_07 should be set as the input mode for this application. PB_07 is also pulled up by an external pull-up resistor on RDB2. If the signal of the PHY changes, the pin may a state change. It is necessary to refer to the manual of the PHY to get more information about this pin signal.
BR
Joey