VR5510 - VIO PIN VOLTAGE INPUT RANGE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

VR5510 - VIO PIN VOLTAGE INPUT RANGE

2,047 次查看
Diwakar07
Contributor III

For the VIO pin of VR5510 we need a voltage range of 1.75 to 3.4V. as show in below image.

Diwakar07_0-1709111451135.png

  We have connected the LDO3 of this same PMIC to supply this pin with 3.3V typical. But during the transient conditions we have a voltage range of +/-6% of typical , which is 3.102 to 3.498V, as shown below.

Diwakar07_1-1709111674163.png

 Is this sort of supply to VIO not advisable? And are we correct in analyzing the transient numbers for the supply inputs?

 

 

0 项奖励
回复
4 回复数

2,021 次查看
Diwakar07
Contributor III

Hi diazmarin09,

   Actually we are not within the range. The maximum output from the LDO3 is 3.498V but the acceptable maximum in PMIC VIO is 3.4V only. Hope this is clear. We want to know if there will be issues due to this.

0 项奖励
回复

1,996 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Diwakar07, 

Your patience is greatly appreciated. 

Please review the response from our specialist below:

Please check below maximum rating for VR5510 pins.

VDDIO (All other pins in the table) maximum rating is 5.5V.  There is no potential issue to use LDO3 to power VDDIO. 

diazmarin09_0-1709259570686.png

I hope this information helps.

Regards,

David 

 

0 项奖励
回复

2,014 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Diwakar07,

I am pleased to contact you again. 

My apologies for the misunderstanding. Now I see your point. 

I will ask internally and will let you know asap. 

Regards,

David 

0 项奖励
回复

2,033 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Diwakar07,

I hope all is great with you. Thank you for using the NXP communities.

Yes, it is. I do not see any issue with your configuration as you are within the range. You are correct in considering the transient load regulation of the LDO3 output voltage.

I hope this information helps.

Regards,

David

0 项奖励
回复