Hello,
I am using goldvip package which is available for S32g3 RDB3 board,
I am trying to integrate Memstack but , fls_init is not happening , its going to exception .
so i thought i need to use Rm module so i can configure XRDC module allowing M7_0 to access the QSPI peripheral .
But i am unable to import this module into EB environment even if i have Rm plugin in the Plugin path, through module configuration .I mean RM module is not visible in the module configuration
Could any one assist me to import this module ,or assist me to use fls effectively without this module.
Regards
Karthik
Hi,
Can you let us know which GoldVIP version are you using?
Please, let us know.
Hello @Daniel-Aguirre ,
I am using GoldVIP-S32G3-1.11.0
Hi,
Thanks for your feedback. We seem to be able to reproduce the situation you are mentioning.
Seems to be that the XRDC features should have been moved to the Bootloader project, since the XRDC is to be initialized at first.
Still, we will confirm whether this is expected under the CAN-GW project or not.
We apologize for any delay from our side.
Please, let us know.
Hi,
We apologize for the delay from our side.
We have received the following update from the internal team:
"You should be able to configure RM modue in the bootloader package. of GoldVIP1.11.0"
Please, let us know.